Back to Main Menu

Create a Template

Objective: Gain an understanding of the ways to create a Template in Predictor 

  • On the portfolio screen, click on Add Template

 

  • Alternatively, right-click the portfolio name and click Add


A template with the given name is created under the portfolio as shown in the following screen:


Templates can be created for different asset categories or asset groups by following a similar procedure.

Existing Templates from different Portfolios can be created in the current Portfolio using the 'Import Template' function from the file menu: